DISPLAY.MONITOR.VALUE

Description

DISPLAY.MONITOR.VALUE is part of the Live Monitor feature and defines the command values that are displayed for each of the user definable channels. Whatever keywork is set to the value will be displayed on the LCD screen next to the label.

There are six channels available, and this keyword is an array so an index must be supplied then the value next. See below for examples

Examples

To retrieve all values simply issue the command:

-->DISPLAY.MONITOR.VALUE

[0] AXIS1.PL.FB

[1] AXIS1.VL.FB

[2] AXIS1.IL.FB

[3] Empty

[4] Empty

[5] Empty

To retrieve a single label, issue the command with an index DISPLAY.MONITOR.VALUE 0:

-->DISPLAY.MONITOR.VALUE 0

AXIS1.PL.FB

To set a single label issue the keyword with index and a value:

-->DISPLAY.MONITOR.VALUE 0 AXIS1.VL.KP

-->DISPLAY.MONITOR.LABEL 0

AXIS1.VL.KP


  • The value must be a valid “readable” keyword – if it is not, an error will be returned and the existing value will not be modified.

Versions

Action Version Notes
Implemented 02-11-04-000

 

General Information

Type Read/Write
Units Sets the command keyword for the Live Monitor channels.
Range N/A
Default Value 32 Characters
Data Type String

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

DISPLAY.MONITOR.VALUE 0

3017h

01h

String(64)

-

-

Read/Write

No

DISPLAY.MONITOR.VALUE 1

3017h

02h

String(64)

-

-

Read/Write

No

DISPLAY.MONITOR.VALUE 2

3017h

03h

String(64)

-

-

Read/Write

No

DISPLAY.MONITOR.VALUE 3

3017h

04h

String(64)

-

-

Read/Write

No

DISPLAY.MONITOR.VALUE 4

3017h

05h

String(64)

-

-

Read/Write

No

DISPLAY.MONITOR.VALUE 5

3017h

06h

String(64)

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

2026

1

2026 (0x7ea)

DISPLAY.MONITOR.VALUE

String[6]

Read/Write

No

PROFINET

Parameter

PNU

Data Type

Access

Units

DISPLAY.MONITOR.VALUE

2026

String[6]

Read/Write

-